Hi again,
I’ve been playing with the tsunami’s syned set function was wondering if the following feature could be added:
A new function: Synced set with bank offset. Basically its the same As the current one but it takes into account the bank value set by functions ‘trigger bank up’ and ‘trigger bank dn’, just like the ‘normal’ function does
The reason for this is as follows:
I use banks for each song or section of a song.
So song1 might have tracks 1-6 for ‘synced set’ tracks, 7-14 one shot sample, and 15 and 16 are configured for bank up/sn
Ideally, i would then like to have tracks 17-22 as ‘syned set’ tracks and 23-30 one shot in bank 2 for song 2, etc etc
That way, when i change bank to bank 2, if i retrigger the synced set, i would get the tracks 17-22, which would indirectly cause tracks 1-6 to stop playing
Currently, i cant do, as if i retrigger the synced set, after changing a bank, it will still play the original tracks 1-6.
I hope this makes sense, and really hope you’ll consider it as a feature!! ![]()
Thanks
Guy