Tsunami Super WAV Trigger one button plays 4 outputs

Can I set it up so I just press one button and it will play 4 sounds from 4 outputs simultaneous and in sync ?
I will use it to play multitrack rhythmic music to 4 separate outputs so the sync is really important.

Jeremy

Do you wish to play all 4 files simulteneously or one by one?

Thanks for your reply.
I wish to press one button that will trigger 4 different sounds to each of their own output simultaneously.
It for audio visual synchronizing so the sync must be spot on.
(DMX/MIDI or likewise is not an option)

This thread might help Tsunami as a matrix switcher?

Yes. There is a programmable trigger function called “Synced Set” that will trigger up to 8 (or 4 stereo) tracks (.wav files) and send them each to a different output. They will all start with the single trigger and be in sample sync. If the tracks are all the same length and looped, they will stay in sync all day long.