Hello Crew,
I’ve gotten the wav trigger working as a media player with tracks playing from one output. I’m getting a bit stuck on setting up the 4 stereo outputs playing 4 synched tracks using trigger one. Does anyone have any advice how to get make this work?
             
            
              
              
              
            
            
           
          
            
            
              Unfortunately I don’t believe you can sync 4 tracks off one trigger.
If your files are all exactly the same number of samples you could trigger 4 trigger inputs all at the same time and they would play in sync though.
             
            
              
              
              
            
            
           
          
            
            
              Hey Chris,
Thanks. What if I hardwire the one trigger to the 4 tracks I want to play and have them assigned to the 4 outputs?
             
            
              
              
              
            
            
           
          
            
            
              You could give that a try, but I don’t know if that’s going to work.
             
            
              
              
              
            
            
           
          
            
            
              If you use the mono version of the firmware, you can use the Synced Set trigger function to start up to 8 tracks in sample sync with a single trigger. The tracks must be sequential and each track will be routed to a separate output. If you convert each of your stereo tracks to mono, then you can start all 4 stereo pairs in sync with a single trigger.
Hope this helps.