TSUNAMI super WAV trigger: Loop issues. 1/2 speed on first repeat.

HI All.

I’m using the TSUNAMI super WAV trigger as an 8ch playback device, playing eight 40-minute mono files on loop. I’m using the Tsunami Mono firmware & the Synced Set function. The ‘loop’ tick box is greyed out when I choose my trigger type as ‘level’ but looking at this forum seems that the config software just runs that way and that it loops automatically as long as my physical switch is set to ON.

All of this is fine when I turn the switch to ON, all 8 mono files play out of their individual outputs and at the end of the 40 mins, it loops back to the beginning. HOWEVER, after the first playback when it’s looped is seems to be playing at 1/2 speed or have odd sample issues. - have you any idea how to solve this?

– INI file:

#TSUM

#TRIG 01, 65, 0, 0, 14, 1, 8


This file was generated by the Robertsonics Configurator v2.00

for use with the Tsunami Mono firmware. It is only required if

you wish to over-ride default settings. You may add your own

comments below this line →

The only way I’ve found so far to solve this issue is to change the Trigger Type to ‘Edge’ (which enables the loop tick box). But now I don’t have the option to turn the loop off using my ON/OFF switch, just re-trigger it (unless I turn off / disconnect the Super WAV trigger).

Using a level trigger and keeping it active just restarts that track after it reaches the end. There will almost always be a 1 to 3 millisecond gap and it won’t guarantee that multiple tracks will stay in sync over multiple restarts.

Using an edge trigger and checking the “loop” box produces a truly seamless loop between the last sample in the track and the first, and tracks of equal length started with the Synced Set function that are looped this way will stay in sample sync through all subsequent loops. You can use the Stop trigger function to stop a range of tracks using a second trigger.

That said, the strange behavior when using the level trigger sounds like a bug. It may be that I’ve never tested using the combination of a level trigger and Synced Set function. Were all 8 tracks affected equally?

Hey, thanks for the quick reply,

All 8 tracks were affected equally.

The 3-millisecond gap is not an issue at all (it’s silent for that part anyway), the main issue is that the audio quality is unusable once it’s re-triggered, slowed down / granular sounding buffer effect. I’ll do it with two buttons for now. Just to note, I’ve tried using previous versions of the WTConfig as 2.0 is a beta, but still the same issue and also different versions of the Tsunami mono HEX files.

@robertsonics

bumping this old thread – i’m similarly interested in level triggered-synced set combination, as it (should) allow for looping play of 7.1 systems in an always-on way.

I don’t get the 1/2 time issue, but the sample buffer/phasing sound issue happens on the second playthrough (the type of align delay sound you get with things sounding slightly more metallic or downsampled), and the third time it actually completely stops playing.

It sounds like the solution is to just move to edge or latch with loop enabled, but if there was ever more debugging of this use-case, it would be a valuable adjustment to the firmware.

Thinking about this now, I realize that level triggers with the synced set function is not something that I ever considered. With Tsunami, level triggers should not be confused with looping - they are completely different. Holding a level trigger active simply causes the track to restart immediately after it finishes, just the same as if you had activated another edge trigger. This includes reloading the first sector of the track and then starting it immediately. The reason this doesn’t work with a synced set is that all the tracks in a synced set have to be preloaded and ready to fire with the resume command. With a level trigger, all the tracks are restarted as if for the first time, and they will definitely be out of sync. In hindsight, I should have prevented this combination.

However, when a track is set to loop, it preserves the first sector in memory and doesn’t need to reload. It simply skips from the last sample in the file to the first and keeps going. If multiple files are all started and looped at the same time, and are the same length, then they will remain in perfect sync until stopped. What the synced set trigger function does is preload and pause all the files first and then issue a “resume all in sync” function, which guarantees all tracks will start in sample sync.