Tsunami Super Wave Trigger - 1 second default audio fadeout?

Hello all.

I’m attempting to use the Tsunami Super Wave Trigger as a standalone audio playback device triggered by contact closure.

I’ve set up my second trigger to start playback of a sound file on a button press but then stop playback when the button is released using the “Level” and “Normal” settings in the trigger options of the configuration utility. This works but I notice that there is what seems to be a default 1 second fadeout of the audio playback vs a hard stop upon release of the button.

Does anyone know if it’s possible to change the default fadeout times in standalone mode? I’ve been through all the documentation and it looks like that functionally may require triggering the device via MIDI.

Essentially I’m trying to mimic Start/Stop playback of the wave file without the need of a separate MIDI device to send a Note On/Off with 0ms release time.