Hi everyone,
I currently using bluetooth or my robot project but due to the NLOS limitation, I’m looking at using um-96 to replace bluetooth. However, I have problem getting the UM-96 modules to work properly. Here are the sequence of my tests, hopefully somebody can give me some hints:
-
Connect to max232 adapter to com 1 of 2 computers
-
Connect RX to TX and TX to RX (TTL)
-
Launch Hyperterminal on both pc, set to com1, 9600, 8n1 then connect to com 1
-
Any thing I type from one hypterminal will show up on the other hyperterm
-
This tells me that the RX and TX works for TTL
-
On 2 um-96, jumpers are settup as follow:
A: shorted
B: not shorted
C: not shorted
D: not shorted
E: shorted
-
Connect GND and VCC to 4.5 V power souce
-
Connect TX of um-96 to RX of max232 and rX of um-96 to TX of max232
-
Power on the um-96
-
On hyperterms of both PC, see see the init string:
uM96V23AXM
-
After that, any thing I typed on a hyperterm will not show up on the other hyper term.
-
The rx lights on the max232 shows no data received when I hit the Enter key to send string from hyperterm.
Can somebody give me some hits of what I did wrong or missing?
Thanks,
Jonathan