Module: u-blox LARA-R6401 (SPARKFUN LTE STICK)
Network: Jio India
Firmware Version: 2.14
Hi everyone,
I’m facing an issue while establishing secure HTTP (HTTPS) and FTP (FTPS) connections on the LARA-R6401 module. After setting up all required parameters, I consistently receive the following errors:
- HTTPS:
Error code 11 – server connection error - FTPS:
Error code 63 – Cannot set secure socket
Debug Steps Taken
- Confirmed root certificate is imported successfully with valid base64 and no PEM headers
- Tried multiple known-good HTTPS and FTPS servers
- Non-secure HTTP and FTP operations succeed
- PDP context successfully shows IP addresses (IPv4 & IPv6)
- FTPS and HTTPS fail consistently when secure option is enabled
- Attempted different SSL profile IDs, DNS hostnames, and APNs
Could you please advise:
- Does LARA-R6401 fully support secure FTP and HTTPS over IPv4/IPv6 in the latest firmware?
- Is there a specific CA bundle required for T-Mobile USA networks?
- Are the errors indicative of a firmware issue, or a module limitation?
I’ve also reviewed the official u-blox AT command examples from this document:
AT-CommandsExamples_AppNote_%28UBX-13001820%29.pdf
2.87 MB
Many of the same errors are mentioned in this , but unfortunately, no resolutions are provided.
Any insights, suggestions, or working configurations would be greatly appreciated.