On Ubuntu 18.04.5 LTS. I am able to successfully do hardware test for CH340C https://learn.sparkfun.com/tutorials/sp … dware-test.
I see the device listed
anil@anil-laptop:~$ lsusb
Bus 001 Device 009: ID 1a86:7523 QinHeng Electronics HL-340 USB-Serial adapter
anil@anil-laptop:~$ ls /dev/ttyUSB*
/dev/ttyUSB0
I am trying to get the Ambiq SDK example to work. Following instructions as described in https://learn.sparkfun.com/tutorials/us … plications
I am unable to upload the built accelerometer example. I selected port 0 and I keep getting Com Port not found - Did you select the right one?. Please help. Commad Line output:
anil@anil-laptop:~/projects/AmbiqSuiteSDK/boards_sfe/edge/examples/lis2dh12_accelerometer_uart/gcc$ make COM_PORT=COM0 bootload_asb ASB_UPLOAD_BAUD=921600
Makefile:112: warning: you have not defined PYTHON3. assuming it is accessible by 'python3'
Makefile:120: defaulting to 921600 baud for SVL
Makefile:125: warning: you have not defined SDKPATH so will continue assuming that the SDK root is at ../../../../..
Makefile:133: warning: you have not defined COMMONPATH so will continue assuming that the COMMON root is at ../../../../common
Makefile:141: warning: you have not defined BOARDPATH so will continue assuming that the BOARD root is at ../../..
Makefile:149: warning: you have not defined PROJECTPATH so will continue assuming that the PROJECT root is at ..
python3 ../../../../common/tools_sfe/asb/asb.py --bin ../gcc/bin/lis2dh12_accelerometer_uart_asb.bin --load-address-blob 0x20000 --magic-num 0xCB -o ../gcc/bin/lis2dh12_accelerometer_uart --version 0x0 --load-address-wired 0xC000 -i 6 --options 0x1 -b 921600 -port COM0 -r 2 -v
Header Size = 0x80
original app_size 0x3fa8 ( 16296 )
load_address 0xc000 ( 49152 )
app_size 0x3fa8 ( 16296 )
w0 = 0xcb004028
Security Value 0x10
w2 = 0x10008080
addrWord = 0xc000
versionKeyWord = 0x0
child0/feature = 0xffffffff
child1 = 0xffffffff
crc = 0x49cfc4e4
Writing to file ../gcc/bin/lis2dh12_accelerometer_uart_OTA_blob.bin
testing: ../gcc/bin/lis2dh12_accelerometer_uart_OTA_blob.bin
Header Size = 0x60
app_size 0x4028 ( 16424 )
Writing to file ../gcc/bin/lis2dh12_accelerometer_uart_Wired_OTA_blob.bin
Image from 0x0 to 0x4028 will be loaded at 0x20000
Connecting over serial port COM0...
Detected Serial Ports:
USB Serial
Com Port not found - Did you select the right one?