Hi, I am trying to set up single makefile target to write flash memory of lpc2148 on
64bit Linux host.
I am able to connect to openocd daemon. In console when I issue commands:
> reset
> halt
> flash write_image erase main.bin 0 bin
everything goes ok right now, but problems start when I try to issue the same commands when starting openocd daemon. The command like this:
$ openocd -f $interface -f $target -c "reset" -c "flash write_image erase main.bin 0 bin"
or
$ openocd -f $interface -f $target -f $flash_script
ends with following error:
Open On-Chip Debugger 0.2.0 (2009-07-26-00:21) Release
$URL: http://svn.berlios.de/svnroot/repos/openocd/tags/openocd-0.2.0/src/openocd.c $
For bug reports, read http://svn.berlios.de/svnroot/repos/openocd/trunk/BUGS
1 kHz
RCLK - adaptive
1000 kHz
jtag_nsrst_delay: 200
jtag_ntrst_delay: 200
Runtime error, file "command.c", line 469:
Unknown command: reset
make: *** [program] Error 1
I am using
-
openocd-0.2.0
-
ubuntu 9.04 64bit
-
gnuarm-4.3.2 build from sources
Could somebody interested help me to solve this out?