I am working on a project to gather biometric data using the Sparkfun Triple Axis Accelerometer Breakout and Sparkfun Oximeter and Heart Rate Sensor - MAX30101 & MAX32664. I am trying to collect and transmit the data on the SparkFun DataLogger IoT. Is it possible to power the accelerometer board with the IOT? I have purchased two accelerometer boards but both of them are not transmitting any data to the IOT board or showing up as connected devices.
Also, is it possible to power the two hardwired connections on the Oximeter board from the IOT Board?