Hi everyone
I am currently performing few experiments (mostly discharge profiles, as my target applications are for wireless sensor networks where charging is not required). The aim is to monitor the discharge profiles of few batteries over different temperatures.
I have a simple circuit, where the sparkfun coulomb counting module draws current, which is read by arduino pro and later logged using CoolTerm on the PC.
To break it down, I will specify some of the experimental conditions and specifications.
The equipment is working as intended and I am able to log all the readings, but, the biggest worry is the battery discharge time, as of now its been 18 hours and the battery State of Charge (SoC) is still at 84%. At this pace, it will take another 4 days to completely discharge the battery. As I have to experiment with 4 different battery types over different temperatures (-10C, 0C, 10C, 20C, 30C, 40C), so if my maths is correct
Time for one experimental run = 5 days OR 120 Hours
Time for one battery with 6 temperature variations = 30 experimental runs
Total number of experimental runs of 4 batteries = 4 x 30 = 120 experimental runs
Total number of hours = 120 x 120 = 1440 hours ![]()
I am not sure what I’m missing here. I know I can buy additional boards and modules and run these experiments in parallel, but still it would cost me months.
I am a little skeptical about the attached load on the batteries, as currently it is 50mA load (because my wireless sensor network draws almost that much load and I wanted to keep it close to it possible).
This is my very first time working with batteries and I am unsure regarding the State of Charge (SoC) values , so I would like to ask the following questions:
So thankful for your time going through my query, any help or pointer is highly appreciated.
cheers