Venus638FLPX serial problem

I’ve had my Venus 638FLPX for several months on my AVC robot with no problems. It was working yesterday just fine. Tonight I went to use it and discovered problems with serial comm. I get gibberish for any baud rates from 1200 thru 230400. This is on the PC using SFE 3.3V FTDI breakout. The robot isn’t able to read NMEA off of it either which is what prompted me to check on the PC.

The GPS is configured for 10Hz output rate and NMEA messages. It was working great for hours last night. I did leave it plugged in and running all night last night but I’ve done that a dozen times before with no problems.

I put the GPS TX line on the scope and the edges look square, and there are pulses coming through and no noise that I could see. The scope I used is very basic so couldn’t isolate a waveform to estimate baud rate. I guess I’ll have to dig out the good scope.

Is there any way to reset it if I can’t communicate with it? For now I’ve pulled the backup battery and am crossing my fingers that tomorrow morning it’ll behave sanely again.

Naturally this has to happen with only a few weeks before the AVC when I’m already desperately battling a new bug that’s jacked up the robot’s nav accuracy. Gotta love it. :roll:

Any ideas of what’s wrong or what I could try?

That was weird. After sitting all night without a backup battery, it works now at the expected 38400. Yay!

$GPGGA,155902.200,2400.0000,N,12100.0000,E,0,00,0.0,0.0,M,0.0,M,0000*61

$GPRMC,155902.200,V,2400.0000,N,12100.0000,E,000.0,000.0,280512,N*76

I just bought this product and i try to use the arduino uno R3 microcontroller to get the standard NMEA output…but i am not able to get any of the output…

only the power LED is on the rest is dead…

can anybody check my code…

seeking help…

i used the tinygps library of arduino…

#include <SoftwareSerial.h>

#include <TinyGPS.h>

/* This sample code demonstrates the normal use of a TinyGPS object.
   It requires the use of SoftwareSerial, and assumes that you have a
   4800-baud serial GPS device hooked up on pins 3(rx) and 4(tx).
*/

TinyGPS gps;
SoftwareSerial nss(3, 4);

static void gpsdump(TinyGPS &gps);
static bool feedgps();
static void print_float(float val, float invalid, int len, int prec);
static void print_int(unsigned long val, unsigned long invalid, int len);
static void print_date(TinyGPS &gps);
static void print_str(const char *str, int len);

void setup()
{
  Serial.begin(115200);
  nss.begin(4800);
  
  Serial.print("Testing TinyGPS library v. "); Serial.println(TinyGPS::library_version());
  Serial.println("by Mikal Hart");
  Serial.println();
  Serial.print("Sizeof(gpsobject) = "); Serial.println(sizeof(TinyGPS));
  Serial.println();
  Serial.println("Sats HDOP Latitude Longitude Fix  Date       Time       Date Alt     Course Speed Card  Distance Course Card  Chars Sentences Checksum");
  Serial.println("          (deg)    (deg)     Age                        Age  (m)     --- from GPS ----  ---- to London  ----  RX    RX        Fail");
  Serial.println("--------------------------------------------------------------------------------------------------------------------------------------");
}

void loop()
{
  bool newdata = false;
  unsigned long start = millis();
  
  // Every second we print an update
  while (millis() - start < 1000)
  {
    if (feedgps())
      newdata = true;
  }
  
  gpsdump(gps);
}

static void gpsdump(TinyGPS &gps)
{
  float flat, flon;
  unsigned long age, date, time, chars = 0;
  unsigned short sentences = 0, failed = 0;
  static const float LONDON_LAT = 51.508131, LONDON_LON = -0.128002;
  
  print_int(gps.satellites(), TinyGPS::GPS_INVALID_SATELLITES, 5);
  print_int(gps.hdop(), TinyGPS::GPS_INVALID_HDOP, 5);
  gps.f_get_position(&flat, &flon, &age);
  print_float(flat, TinyGPS::GPS_INVALID_F_ANGLE, 9, 5);
  print_float(flon, TinyGPS::GPS_INVALID_F_ANGLE, 10, 5);
  print_int(age, TinyGPS::GPS_INVALID_AGE, 5);

  print_date(gps);

  print_float(gps.f_altitude(), TinyGPS::GPS_INVALID_F_ALTITUDE, 8, 2);
  print_float(gps.f_course(), TinyGPS::GPS_INVALID_F_ANGLE, 7, 2);
  print_float(gps.f_speed_kmph(), TinyGPS::GPS_INVALID_F_SPEED, 6, 2);
  print_str(gps.f_course() == TinyGPS::GPS_INVALID_F_ANGLE ? "*** " : TinyGPS::cardinal(gps.f_course()), 6);
  print_int(flat == TinyGPS::GPS_INVALID_F_ANGLE ? 0UL : (unsigned long)TinyGPS::distance_between(flat, flon, LONDON_LAT, LONDON_LON) / 1000, 0xFFFFFFFF, 9);
  print_float(flat == TinyGPS::GPS_INVALID_F_ANGLE ? 0.0 : TinyGPS::course_to(flat, flon, 51.508131, -0.128002), TinyGPS::GPS_INVALID_F_ANGLE, 7, 2);
  print_str(flat == TinyGPS::GPS_INVALID_F_ANGLE ? "*** " : TinyGPS::cardinal(TinyGPS::course_to(flat, flon, LONDON_LAT, LONDON_LON)), 6);

  gps.stats(&chars, &sentences, &failed);
  print_int(chars, 0xFFFFFFFF, 6);
  print_int(sentences, 0xFFFFFFFF, 10);
  print_int(failed, 0xFFFFFFFF, 9);
  Serial.println();
}

static void print_int(unsigned long val, unsigned long invalid, int len)
{
  char sz[32];
  if (val == invalid)
    strcpy(sz, "*******");
  else
    sprintf(sz, "%ld", val);
  sz[len] = 0;
  for (int i=strlen(sz); i<len; ++i)
    sz[i] = ' ';
  if (len > 0) 
    sz[len-1] = ' ';
  Serial.print(sz);
  feedgps();
}

static void print_float(float val, float invalid, int len, int prec)
{
  char sz[32];
  if (val == invalid)
  {
    strcpy(sz, "*******");
    sz[len] = 0;
        if (len > 0) 
          sz[len-1] = ' ';
    for (int i=7; i<len; ++i)
        sz[i] = ' ';
    Serial.print(sz);
  }
  else
  {
    Serial.print(val, prec);
    int vi = abs((int)val);
    int flen = prec + (val < 0.0 ? 2 : 1);
    flen += vi >= 1000 ? 4 : vi >= 100 ? 3 : vi >= 10 ? 2 : 1;
    for (int i=flen; i<len; ++i)
      Serial.print(" ");
  }
  feedgps();
}

static void print_date(TinyGPS &gps)
{
  int year;
  byte month, day, hour, minute, second, hundredths;
  unsigned long age;
  gps.crack_datetime(&year, &month, &day, &hour, &minute, &second, &hundredths, &age);
  if (age == TinyGPS::GPS_INVALID_AGE)
    Serial.print("*******    *******    ");
  else
  {
    char sz[32];
    sprintf(sz, "%02d/%02d/%02d %02d:%02d:%02d   ",
        month, day, year, hour, minute, second);
    Serial.print(sz);
  }
  print_int(age, TinyGPS::GPS_INVALID_AGE, 5);
  feedgps();
}

static void print_str(const char *str, int len)
{
  int slen = strlen(str);
  for (int i=0; i<len; ++i)
    Serial.print(i<slen ? str[i] : ' ');
  feedgps();
}

static bool feedgps()
{
  while (nss.available())
  {
    if (gps.encode(nss.read()))
      return true;
  }
  return false;
}

Hi Razeyprolink,

Please shoot us an email at techsupport@sparkfun.com. It may simply be a bad chip on your module. One thing to try would be to hook up directly to the GPS unit, using a USB to serial adapter, such as an FTDI breakout board if possible. If you can’t get any serial data out this way, it is likely an issue with the Venus unit.

If you can email us with a description of how you have everything hooked up, any output you are able to get from the module, and your order number, we can help you out.

Thanks!