I’ve looked over all the troubleshooting material I can find.
Slow red blinking LED.
Switch is in run position.
SD card is V10 32 GB, but I’ve also tried a 2 GB card.
Renamed files to 001.wav, etc. Tried with just one file.
Audio amp is checked.
I power cycled between each change.
So far neither button nor trigger produces any sound.
Thanks for any help you can offer.
Mark
             
            
              
              
              
            
            
           
          
            
            
              Also ensure there is 0 metadata for the file (image, info, etc)…you can use audacity to strip it out (or use the ones here https://cdn.sparkfun.com/assets/learn_t … umbers.zip and that the files is in to root directory of the SD card
There are more things it could be listed on pg 14 here https://cdn.sparkfun.com/assets/1/c/9/a … 230114.pdf - be sure to rule those out too
Here’s our guide https://learn.sparkfun.com/tutorials/wa … #operation as well
             
            
              
              
              
            
            
           
          
            
            
              Thanks so much for the advice. I had saved the files without metadata, but something must have crept in. I ran everything through Audacity and it works a treat now.
Cheers