Can I know if a track is done playing. What I want to do is loop a track with variable pitch (external control via N_pitch). When using samplerateOffset() the play duration changes. Using trackLoop() and PlaySolo() doesn’t work well.
wTrig.trackLoad(11);
wTrig.trackLoop(11, 0);
wTrig.trackPlaySolo(11);
wTrig.samplerateOffset(N_pitch); // varies between -32k and +32k
delay(400); // duration of track (normal pitch) is 1 sec.
wTrig.trackFade(11, -20, 20, 1);
             
            
              
              
              
            
            
           
          
            
            
              How can I know track duration of a WAV file (at normal speed)?
             
            
              
              
              
            
            
           
          
            
            
              What I mean: to know the duration before playing the track. Something like wTrig.duration(track);
             
            
              
              
              
            
            
           
          
            
            
              Is it possible to add these functions:
- 
wTrig.trackDuration(track) : returns track duration in ms 
- 
wTrig.trackPlaying(track) : returns TRUE while track is playing 
- 
wTrig.trackFile(track) : returns TRUE if the file is on the SD-CARD 
- 
wTrig.setBank(bank) : sets a sound bank. A bank is like a folder. Default is 0. A convenient way to subdivide and access sounds 
 
            
              
              
              
            
            
           
          
            
            
              That would be great. I’m working on this art project called The Ommegang (the procession) - Time Spirits where a new instrument is central: the macePod.
The first performance is in the centre of the city of Ghent on April 23rd.
And another: negative pitch values to play the tracks in reverse…
Read more here:
https://stad.gent/kunst-op-straat/nieuw … imesprites
Crowdfunding:
https://crowdfunding.gent/nl/projects/t … e-ommegang
             
            
              
              
              
            
            
           
          
            
            
              The best way to let samples play in reverse would be to set a flag: wTrig.trackDirection(int); -1 for reverse, 0 for pause, +1 for forward. Could be used to set speed too.