I have 5 WiFly RN-XV modules. Four of which are configured as client to the 5th one which acts as host. Each of them connects with the host to transmit/receive data and after a given idle time, it disconnects so that the other modules can create a socket. However, I want to my host to create multiple sockets with with its clients so that it can communicate simultaneously. Also i have an android app which communicates with the host module. Is there any way by which I can open multiple tcp connections ???
Related topics
Topic | Replies | Views | Activity | |
---|---|---|---|---|
RN-XV Wifly multiple posts without closing TCP connection? | 0 | 476 | September 17, 2013 | |
RN-XV WiFly Module | 3 | 1129 | December 10, 2014 | |
SparkFun Bluetooth Modem - BlueSMiRF Silver multiple connections | 1 | 5156 | November 10, 2020 | |
Another RN-171XV Wifly connection problem..... | 2 | 1022 | August 18, 2013 | |
Wifly GSX breakout question | 6 | 1433 | January 10, 2010 |