Will SparkFun carry the 14-pin double-insulator header?

PJRC sold a 14-pin double-insulator header that is used to mount a Teensy 4.1 onto an OctoWS2811 board. (PJRC Store). They’re necessary because shorter pins don’t work. See pictures and notes here: PJRC Store

Will SparkFun sell these at some point, and if so, when might that be? (Even longer lengths than 14 pins are acceptable; I can cut them.)

I asked around and…yes! We’re just waiting on photos to get uploaded and then they’ll be added to the site, it should be in the next few weeks if you can hold out a bit more

Thank you for the reply.

They are now live! Double Insulated Header Pins - 14x1