WinArm doesn't find example file.

Greetings friends.

Two questions. First about the Logomaticv2 I’m trying to reprogram. Can I drop the FW.SFE file on the SD chip directly to modify the boot sector as I need…?

Second about the winarm compiler, I downloaded winarm20060606 and installed it in C:winarm\ then changed the path in computer setup as required.

Directory of Winarm: C:\WinARM\

Now the Programmer Notepad gives me this on every file I try to compile.


“make.exe” all

make.exe: *** No rule to make target `all’. Stop.

Process Exit Code: 2

Time Taken: 00:00


Obviously it’s not working right. The full path is:

%SystemRoot%\system32;%SystemRoot%;%SystemRoot%\System32\Wbem;C:\Program Files\Intel\DMIX;C:\Program Files\Microchip\MPLAB C32 Suite\bin;C:\Program Files\QuickTime\QTSystem;C:\WinARM\utils\bin;C:\WinARM\bin

I’m now at this, and need help with getting the Logomatic working for me.

Thanks for your help.

On winarm, there’s a section for it and help, on the user forum at avrfreaks.net

Thanks will check it out.