WiTilt V2.5 configuration menu problem

Dear All

i bought Wireless Aceelerometer/Tilt Controller version 2.5.

i can connect it from hyperterminal and self written program.

But one thing make me very inconvenient because we are planning to give participants to use.

First time Witilt is connected, it will send configuration menu block

WiTilt V2.5, Firmware V4.2 - Configuration Menu:

=========================

[1] Start Tri-Ax detection (hit spacebar to stop)

[2] Set Active Channels (XYZ Active)

[3] Calibrate

[4] Sensor Range (+/-1.5g)

[5] Display Mode (Raw)

[6] Set Threshold (Currently +/-0.0g)

[7] Set Output Frequency (40Hz)

[8] Set Bluetooth (Currently Active)

and then i send “1” for reading x,y,z data. And then send spacebar to stop reading data. After sending spacebar, witilt will also send again configuration menu block. Then i disconnected witilt from hypertermianl or self wirtten program.

Second time, i connected to Witilt again. at that time, it will send three times of configuration menu block. After that i send “1” for reading data , it will not respond. i have to click reset button.

Actually it is very inconvient for users to use. i am wondering is there anyway i can control so that everytime the accelerometer is connected, it will send one time of configuration menu block and no need to click reset button.

thanks a lot for helping me

rodent