I have some breakout boards for this module. It has the full 36 pin interface in a dip package or you can use just the edge in a 4 or 8 pin configuration (which is all you need to use its wifi functions).
I delivered some to OP and AFAIK, he had no problem getting them to work.
The board has the full 40 pin interface or a “sideways” interface that is 3-8 pins depending on what capabilities you need. Note that it only supports the data end of the wiz610, not the mechanical end.
There are pads for a “busy/ready” led as well, though you can leave it off. The rest of the support parts are there, caps, resistors, etc.
axzi:
I have some breakout boards for this module. It has the full 36 pin interface in a dip package or you can use just the edge in a 4 or 8 pin configuration (which is all you need to use its wifi functions).
Do you have any more for sale or point me in the right direction. Arduino compatible preferred but not necessary