Hello!
I have here an OpenLog device, with the legend of DEV-13712 on it’s retail packaging. The getting started page (or pages) shows two specific Arduino devices. I have here a RedBoard PTH that is one of them. I do not have the other one. Besides that one, would any of the members, not a MKR type, work with the device? :?:
I can see that wiring it, and following the instructions, will be interesting. :roll:
Openlog is a 3.3V module. It can be connected directly with Arduino pro mini 3.3V. For 5V Arduino boards, you have to use logic level converter.
tepalia02:
Openlog is a 3.3V module. It can be connected directly with Arduino pro mini 3.3V. For 5V Arduino boards, you have to use logic level converter.
So that means it should work with all of the 3.3V ones such as the MKR1000 device? :?:
OpenLog will work with any 3.3V MCU and, using logic level converter, any 5V MCU.
doctorwho8:
tepalia02:
Openlog is a 3.3V module. It can be connected directly with Arduino pro mini 3.3V. For 5V Arduino boards, you have to use logic level converter.
So that means it should work with all of the 3.3V ones such as the MKR1000 device? :?:
Yes. It will work with MKR1000 directly.