Xbee Factory reset without serial communication?

You can do it without a dev board.

It is possible when using the USB board. You just have to go about it in a different manner.

  1. Take the module out of the interface board.

  2. Connect the interface board to the computer.

  3. Open X-CTU

  4. Go to “Modem Configuration”

  5. Put a check in the “Always update firmware” box

  6. Select proper modem from drop down menu,

  7. Select proper function set and firmware version

from drop down menus.

  1. Click on the “Write” button. After a few seconds of

trying to read the modem, you will get an Info box

that says Action Needed. At this point, CAREFULLY

insert the module into the interface board.

  1. You may get the info box again a short while after,

just use the reset button on the interface board.

This should get you back up and running.

It can take a couple of tries but it worked for me.

If you just have a breakout board make sure you hook up the Xbee like this:

http://www.faludi.com/itp_coursework/me … grade.html

It won’t work with just just Dout and Din connected. Otherwise follow the instructions above.

I took this info from this post:

viewtopic.php?p=74970#74970