XBEE PRO 2.4 config file request

Hi

I purchased 2 Xbee 2.4 pros from spark fun. One had an SMA connector whilst the other had a wire antenna.

I messed with XCTU on one of the units and now its transmitting with a delay.

here is the bad config I currently have. Can sparkfun share with me the config file

for “Router END device”?

I used to put this transmitter which had a wire antenna on the UDB on the plane , it works quite fast

now I need to recover the settings. I swapped the 2 units now with Router end device on the ground

and the At coordinator in the plane and everything works great… However I want to have the Xbee with SMA on the ground… so I still need to recover the profile.

ground

XBP24-B_ZigBee_1247.mxi

80

0

261

1247

0

[A]ID=234

[A]SC=1FFE

[A]SD=3

[A]NJ=FF

[A]JV=0

[A]DH=0

[A]DL=FFFF

[A]ZA=0

[A]SE=E8

[A]DE=E8

[A]CI=11

[A]NI=

[A]BH=0

[A]AR=FF

[A]DD=20000

[A]NT=3C

[A]NO=0

[A]PM=1

[A]EE=0

[A]EO=0

[A]BD=4

[A]NB=0

[A]RO=3

[A]D7=1

[A]D6=0

[A]SM=0

[A]ST=1388

[A]SP=20

[A]SN=1

[A]SO=0

[A]D0=1

[A]D1=0

[A]D2=0

[A]D3=0

[A]D4=0

[A]D5=1

[A]P0=1

[A]P1=0

[A]P2=0

[A]LT=0

[A]RP=28

[A]PR=1FFF

[A]IR=0

[A]IC=0

[A]V+=0

[A]CT=64

[A]GT=3E8

[A]CC=2B

With XCTU, you may reset the XBee config to the factory defaults.

Hi

Its the factory default that is causing the problem…

Allan

A better explanation of what its not doing, doing wrong and you need it do would help.