I wonder if anyone has the same problem as me. I’d like to connect XBee3 Pro on Sparkfun XBee Explorer Regulated board on a PCB shield with Arduino Mega 2560 acting as an end device. However, XCTU could not detect the XBee device. I checked that I had the correct value data/updated drivers and firmware installed but nothing worked. I also checked if there was any problem with the correct Serial port connection, Baud rate, or values setting but still could not detect it with XCTU. The power LED on the board is On, XBee nose is in the correct direction. I also tried testing to connect XBee3 Pro directly with Arduino which can be detected with no problem.
On the coordinate side, another XBee3 Pro to the Sparkfun XBee Explorer USB has no problem with XCTU. I don’t know if the XBee Explorer Regulated module board was broken or if I can do something else to fix this issue.