Hi all,
I am using the ADH8066 Eval board and Module along with the 5V 1A Wall adapter that SF sells.
When I do not have a SIM card inserted into the module it behaves as expected. Not many of the AT commands work, but I can check signal strength and do a few other small things…
When I insert the sim card it seems to work fine for a moment (I have about enough time for AT+CPIN?) but then it spits out a bunch of what appears to be debugging information and resets.
àààü€IIIIw
Ready
AT+CPIN?
+CPIN: READY
OK
CPSR=80000097,LR=00156b80,SP=2001c838,SPSR=0000003f,SLR=00156c09,SSP=0100dcd0,LR
FromPreviousMode=deaddead,r0=00156b80,r1=00000700,r2=0100328c,r3=0000000c,r4=010
0328c,r5=01000c7c,r6=0000000d,r7=00000709,IER=7ffb,PIR=0000,ICR=73ff,IMR=00,IID_
FIQ=0b,IID_IRQ=04
interrupt priority level:
EXT2/EXT3=1, EXT1=1, ONOFFSTAT=1, KBS=1,
TIM_INT=1, UART1_STAT=1, UART1_TX=1, UART1_RX=4,
UART0_STAT=1, UART0_TX=1, UART0_RX=4, SIM_STAT=5,
IIC_STAT=1, DSP_REQ=2, FRAME=3, NMI=7
type=01; v_ModuleNumber=3d, v_FileNumber=01, v_ProcedureNumber=00, v_LocalErrorC
ode=17, v_din_NbGeneralDefense=00
I hit enter after the OK returned from the CPIN query.
Perhaps the 5V 1A supply isn’t adequate? I also tried a 12V 1.5A supply I had kicking around… same error. ![]()
Any ideas what could be causing this? thanks.
Sam