im am aware from where i bought an arm jtag parallel debugger
that it uses openocd
well i have a clone skybox s12 receiver and has a timebomb for it where the product stopped working after flashing it with the usb
so im guessing it uses 14 pin output where i set the pins from the 20 pin to 14 pin layout to the skybox s12
im trying to re flash it with arm jtag ahc244 chip on it with the pin layout
but am not sure how to do it from command prompted for this arm jtag chip
the last thing i tried was putting openocd-0.5.0 on the c drive
then openening by cd c:\openocd-0.5.0 and cd bin and
so then
c:\openocd-0.5.0\bin>
im sure i need to learn something like setting up the arm jtag cfg file that corresponds to the adapter ahc244 first right?