Hey all — I’m having a weird issue with an Alchitry Au V2 and wanted to see if anyone has run into something similar or can provide assistance.
I received the board two days ago. Initially plugging it into USB it had a default LED sweep animation. I was able to program it once over Alchitry labs to do my own simple LED-walk “Hello World” binary that worked just fine. Between that and my next programming attempt the board lost power and was unable to communicate to the computer. No soldering or hardware modifications were done, and it was only ever plugged into a computer USB-C port.
It was working normally, then suddenly stopped powering from its own USB-C port. I tried multiple cables and USB ports and now get no LEDs at all. I also have the Alchitry FT+V2 usb-extender board, and when powering through that I am able to partially power the AuV2 but it is not functional.
A few measurements/details:
-
About 40 mV across the Au V2
+/-power points when powered from its own USB -
About 360 ohms between
+and-with the board unplugged -
If I connect an FT+ V2 and power through that, I get about 4.7 V on the Au’s
+/-points -
In that state the Au lights a few LEDs in a weird pattern and gets noticeably hot
-
With both USB connections present, Alchitry Loader still detects the Au V2 and lets me program it, but a simple LED walking bitstream that was previously working just flashes all the LEDs once and stops
I’ve already opened a support request with SparkFun and emailed Alchitry, but I’m curious whether anyone here has seen a similar Au V2 power/regulator failure or if sparkfun personel here can help me initiate an RMA for this.
Thanks!
Daniel