Trying to find a US supplier of the below starter kit. It would need to be able to support one base station and multiple rovers. There are so many components on sparkfun, I’m a little overwhelmed trying to piece it together.
The Starter Kit XLR allows simple and fast evaluation of Dual Band GNSS RTK technology, based on u-blox ZED-F9P module. Up to 50km LOS!
Est. reading time: 2 minutes
Is this the same?
Thoughts?
Jay
That’s near perfect…we achieved 15km using this antenna on the Tx LoRa Fiberglass Antenna Type N - 5.8dBi (902-928MHz) - WRL-15597 - SparkFun Electronics (with the included 1/2 wave on the Rx); you could probably increase that a bit using that 5.8 dBi antenna on both sides. Also note you’d likely need 2x of Interface Cable N to RP-SMA Cable - 1m - CAB-14911 - SparkFun Electronics if’n
But other than that you’ve got it
Thanks TS -
I was able to get it up and running without the CableN. The antenna side was connected internally and cannot be disconnected.
I have a few questions outstanding but wow. This thing locks on fast and doesn’t lose RTK Fix almost ever.
Thanks!