Connect 2 SparkfunGNSS RTK Facet antennas

Hello,

I have 2 Sparkfun GNSS RTK Facet antennas, I would like to base one and use the other to have accuracy in difficult area. How can I do?

Thank you.

You have to Connect to the GNSS module using the SparkFun Serial Basic Breakout or a similar FTDI cable via USB. Then using a terminal program, you need to Access the module’s configuration via the UBlox protocol. You’ll have to Configure the GNSS module to operate as a base station. Then you’ll have to configure the rover. After that you’ll have to set up a link between the base and the rover.

Set one as a rover and one as a base, and pass the data over BT

Hello,

Thank you, how do I connect the base station to the rover?

Sincerely.

Connecting Bluetooth - SparkFun RTK Product Manual is a good method
Note that you’ll connect 2 devices, 1 as base and 1 as rover and configure their NTRIP/correction source(s) accordingly (which is the next section of the guide…take your time and continue going through the next few sections and you’ll be all set!)