AVR Raven demo kit

Im trying to upgrade the firmware on the raven boards using ISP. I was successful using the .05 header on the board with the .05 to .1 dongle thing to upgrade the 3290 but not with the 1284. After looking into it more it looks like the ISP header on both of my boards is incorrect. VCC(pin 2) and GND(pin 6) are not connected to anything. I tested all the other pins in the header back to the chip and their fine.

Is there a reason the power pins on the ISP header for the 1284 are not connected? Am I missing something?

Yes there is a problem.

http://www.avrfreaks.net/index.php?name … ic&t=65512