Hi all,
I have a bluesmirf (BS) gold. I was originally configuring the module via bluetooth. For a variety of reasons I now want to configure the module locally via a serial cable. I see a number of people in these forums have successfully done this, but I must be a little dimmer than most. :idea:
I bought a MAX232, wired it and connected a serial cable from my PC COM port to the IC. I shorted RX and TX and sure enough in hyperterminal what I typed is what i saw. I then powered the BS with 5V and grounded it. I also shorted RTS and DTR. I then took the RX and TX pins and connected them to my MAX232 (and yes I’ve tried switching them).
I open the COM port and the red light keeps flashing - no green solid light. I try sending “$$$” and no reply. ![]()
-
Am I on the right track with this configuration?
-
Should the flashing red light turn green when I open the PC COM port like it does via bluetooth?
-
Could anyone please share in detail their experience with local configuration?
-
Failing all this, has anyone got a simple method of performing a factory reset of the module?
thank you kindly.
SOLUTION******
Okay folks, if anyone is interested here was the problem. I had programmed the bluesmirf remotely to use a baud rate of 920k. Once I issued the ST,0 command I was doomed because the MAX232 cannot communicate at this baud rate. I therefore did a hard reset. The procedure is found here:
http://www.societyofrobots.com/robotfor … pic=4118.0
Basically find PIO4, power it to 3.3V, power the bluesmirf, then toggle power to that pin 3 times. PIO4 is found as the third pin away from the blue antenna on the side with the most pcb traces.
I then was able to use my MAX232 setup to communicate locally with the unit, but still no green light. i am thinking maybe this has to do with shorting the rts and dtr??
cheers.