CAD for MicroOLED Breakout Board?

I’m working on a little project using these neat Qwiic micro-OLED breakout boards, but I can’t find any CAD drawings for the display itself. I’d really like something that shows the precise overall dimensions and the location of the pixels within that area.

Note I’m asking about the display itself, not the breakout board it’s stuck to.

TIA!

So, here’s a guestimate:


0.66 inches wide / 64 pixels = 0.0103125" per pixel, so extrapolating…
0.0103125 * 48 pixels tall = 0.495"

So 0.66" x 0.495", with a border of approx 1.77mm or 0.07"

Thanks for that. Is there no data sheet for the display itself?

Not for that specific display

Can you give me a manufacturer and part number? I can reach out to them to ask.