Is information available on the specific dimensions of the SparkX Qwiic Alphanumeric Display (SPX-16427). Like board size, display size, hole locations/sizes? There is a lot of stuff in the Documents tab at https://www.sparkfun.com/products/16427, but nothing that obviously has what I was looking for.
In the document tab, there are the Eagle files. You can download a free version of Eagle or import it into another CAD program such as KiCAD.
The board is 1.6" x 1.1". Holes are on 1.4" and 0.9" spacing, 0.13" in diameter. The display is 1.575" x 0.625"
/mike