Cannot charge an iPhone 16 using two USB-C breakout boards

I have a project where I am using two USB-C horizontal breakouts with all 6 wires connected to both breakouts.

When I connect a USB-C cable between a power charger and my dev board and a 2nd USB-C cable to my iPhone SE (using a USB-C to Lightning adapter), I can charge my phone.

However when I try to connect my iPhone 16 without the Lightning adapter, it won’t charge. It will charge if I unplug the iPhone 16 from the dev board and plug in a MagSafe charger pad, the iPhone 16 will charge from that.

Has anyone come across this before?

It sounds like the adapters have an internal IC or something that negotiates with the Apple device and needs it there to function normally

I ordered another USB-C horizontal breakout and after some more experimenting, I ultimately found that if you remove the two 5.1K resistors on the CC1 and CC2 pins, it will charge the iPhone 16.

I ordered a couple more breakout boards for USB ports from Sparkfun–one was a USB Type A female and I verified that if you plug a USB Type A to USB-C cable, that it will charge the iPhone 16.

Awesome! Good job

Hello, I read this with great interest as I have two USB-C sparkfun connectors with the same problem. I followed the advise to remove the 5.1k resistors but alas did not do the trick for me.
I have a super simple case, as I just have vbus and ground connected between then two boards: usb-c in from charger and I was hoping to get charge function from the other board. I also feed a small fan from this setup , cannibalising from the connection between the board (which is the reason for this setup).

Do I need some connection on the other pins to get things to work or is something else wrong with this?

Not usually, but Apple products seem to prefer Apple chargers :-/ Does it work as expected with other usb-c devices?