I just pulled this out of the package. I’m using the SparkFun USB Serial programmer, with 0011 and 0012 Arduino IDE software. When I plug the programmer into the pro mini, (with power and TX/RX, or with just power) the red LED on the board stays lit, the green one starts blinking progressively faster, then stays stale for a few seconds, then repeats. I can’t write to it. I keep getting this error code:
What does this mean? I have the correct com port setup. Tried hitting the reset button before programming it, and i set the “Set RTS On Close” option in windows. Nothing seems to be working. All it does it flash that light. I did try removing the jumper on the programmer, and it kept the green light on the controller solid until I reapplied the jumper, then it went right back into its cycle of flashing the light.
and am trying to program the arduino. Do I need to manually reset? If so when? I have tried 1000 different reset times. You seem to suggest that I need to connect the reset pins together, but I can’t seem to find the reset pin on the Serial USB board.
Also, what configuration do the RX and TX pins have to be connected? RX of Serial USB to TX of Arduino? Or should it be the other way around?
This is really getting me to too! Just like the above situations, I just can’t get it to program, and I’m sure it’s to do with the reset. Any help would be gratefully received, before I grind the mini borad into dust :evil:
I had a similar situation where the stk500_getsync() errors while attempting to program it were occurring. The auto programming reset did not seem to be working and I did the following and it worked.
In the Arduino IDE, upload the code to the Pro Mini device. Immediately after hold the reset switch for a solid second or two and release it.
For some reason this worked for me. Hopefully it helps someone out there.
Okay, I had some more problems, but I think I’ve worked out a definitive solution!
You can get the auto-reset to work with this board by soldering a wire into the hole immediatly below the left header pins (when looking at it with the usb port at the bottom - it connects to pin2 on the chip), and connecting this to the hole marked ‘GRN’ on the arduino mini pro
you need to connect the +ve and gnd on the top of the arduino mini pro to the correct pins on the board as shown here
I had the same problems on Vista and also XP using an Sparkfun FT232R USB board on several computers. Now I use an RS-232 to TTL converter and it works great now.
One other thing : Be carefull, there seem to be 2 pinning-variants for the Arduino Pro Mini. BLK and GRN on my arduino is with BLK near the RXD pin, on the photos I always see GRN on that side !!!
pcrom:
I had the same problems on Vista and also XP using an Sparkfun FT232R USB board on several computers. Now I use an RS-232 to TTL converter and it works great now.
One other thing : Be carefull, there seem to be 2 pinning-variants for the Arduino Pro Mini. BLK and GRN on my arduino is with BLK near the RXD pin, on the photos I always see GRN on that side !!!
Howdy,
I’m doing the same as you - using an RS-232 to TTL converter. I’d rather not use USB for my application.
Might I ask how you managed to get your board to auto reset? Did you connect RTS to the GRN pin?