I have a problem that is bothering me. I have an application running on my Win8 Tablet that communicates with four Arduinos (2x Uno, 1x Mega, 1x own PCB with FTDI). As the Tablet has only one USB-port I have to use a hub to connect to all four boards. So far so good, but every once a while the COM-ports of the Arduinos get lost after restart of Windows and only the FTDI is available at the same COM-port.
Does somebody know if this is a problem of the ATmega16U4 (on the Uno boards) or of the hub or a Win8 specific problem?
The RedBoard combines the simplicity of the UNO’s Optiboot bootloader (which is used in the Pro series), the stability of the FTDI (which we all missed after the Duemilanove was discontinued) and the R3 shield compatibility of the latest Arduino UNO R3.