I having issues getting my RedBoard Turbo to work with Arduino. When the RedBoard Turbo is plugged into the USB port no COM port is assigned, I do get an entry in the device manager as follows
Other Devices
Sparkfun RedBoard Turbo
Sparkfun RedBoard Turbo
Both entries have yellow warning icons next to them
The drivers for this device are not installed. (Code 28)
There is no driver selected for the device information set or element.
To find a driver for this device, click Update Driver.
No com port assigned.
Using Windows 7 64 Bit
Arduino IDE 1.8.8
I have both of the following board definitions loaded
Arduino SAMD Boards (32-Bits ARM Cortex-M0+) 1.6.20
Sparkfun SAMD Boards 1.5.4
I can select the board from the list, but no com ports show up to select from the Port list
Any suggestions as what to do.
Thanks Steven