I’m connecting the above motors (DG01D-E) to the sparkfun auto phat, and I’ve isolated one of the connectors on one of the motor cables as defective. Can I order just another cable (I don’t see this on the website)? Can I get one under warranty? I ordered the motors last year and they didn’t work, so I used something else because I was on a strict timeline.
Defective: Can cables for the Hobby Motor with Encoder - Metal Gear (DG01D-E) be ordered seperately?
We have a 30-day warranty on all products (longer on certain ones!); unfortunately this wouldn’t be covered after such a period between
The motor side is a 6-pin 2.0mm pitch JST connector, the board-side is 6-pin 1.0mm pitch JST connector…we don’t sell replacements currently, but you should able to find one (or I suppose grabbing a motor as an alternative, then you’d have a spare). Or fashion one from spare parts! ![]()