EAGLE How to place the same component in different sheets

Hello, i’m starting with EAGLE.

Just i’m following the tutorial manual, and i have the issue related in the topic.

For instance:

I have a large component, and i want to use the 1-10 pins in sheet 1, and the next 11-20 in sheet2.

In both sheets, i want to see the component completely. (at the moment as the tutorial shows you can separate the component in different parts)

I tried using the invoke command, but just i can show only where it is placed, and not “duplicate it”.

I assume that if i connect the same pin twice, the ERC will notice me with a warning or something like that.