EAGLE - Mirror without moving connections...

Making a schematic, got it practically done, realized I “placed” and connected a bunch of MOSFETs backwards, specifically placed 38 N channel MOSFETs with the source and drain reversed on the schematic.

Not gonna work very well that way.

Looking for a way, in EAGLE, to ‘mirror’ the component on the schematic without changing the connections.

For example, the way it is now, the gate is up, drain points left, source points right.

I want the drain and source to swap positions, without having to disconnect and reconnect the wiring on each component.

If you hooked up the nets wrong, you have to disconnect them and re-draw the nets. I hope with 38 MOSFETs you are using the naming convention and not using full net wires…

Ya, that’s what I ended up doing…just deleting and starting over. I had a method for naming the parts and nets (48 not 38)…4 rows, 12 columns, A thru D, 1 thru 12…S D and G suffixes.

Didn’t take as long as I thought it would…'specially after I figured out a decent method of copying everything.