Failure in Wifi Config when using base coordinates saved in SD in GGG MM SS.ssss format

Failure in Wifi Config when using base coordinates saved in SD in GGG MM SS.ssss format

When trying to add coordinates previously saved in the base coordinates file in GGG MM SS.sssss format, they are copied to the boxes incorrectly.

The Facet detects the spaces between GGG and MM and SS.ssss and copies the degrees in latitude, the minutes in longitude and thus fills in boxes.

I am on version 3.8, which is the one that works best for me in my activity, where I almost always use the base Facet.

I already started a Github entry, but I present it here because not all users enter Github.

I await comments.

Greetings

Creating a github issue is what I was going to advise; that has the best chance of being noticed and addressed

Of course, I’m an old facet user.

Post here to see if more users have gone through the same thing and on Github so that the software is corrected.

Thank you.