Today i had troubles entering WiFi mode after using the facet as a base emitting corrections via WIFI. Unit correctly emitted corrections, but later when i tried to enter WiFi mode it’s shows an IP of 0.0.0.0 i Had to switch to another profile that was not using NTRIP server, and correctly entered WiFi config from there.
I downgraded to v3.5 and deleted all microSD files, now wifi config is working again. I’m gonna update and see, I suspect something in the microSD card was causing troubles.
I suspect there is a bug in v3.8. There was a big change between v3.5 and v3.8 with how we utilize WiFi. Please feel free to use v3.5 for now. And if you have the time, please file an issue on the repo describing how v3.8 is failing.