Hi there,
Both of the UM96’s have sent back the correct serial string to a PC.
Com2 port on both UM96 seem to be working correctly.
As already stated I have got the 2 UM96 to communicate withe each other
from one PC to another PC running hyperterminal at 9600,8,N,1.
The problem I am having is with Com1, allthought they are communicating with each other, what I am sending out, I am not receiving on the other end.
When I used a wire link between the two PICs from uart to uart, the comms were perfect. Therfore I knew what I was sending was correct.
When I replaced the wire with the wireless modules UM96, I did not get the correct result.
Can you confirm the correct jumper settings for 9600, and pin wiring to run at 9600,8,N,1.
If I get time I will connect a level shifter from the PIC and connect it to com2 on the UM96 and the same on the other PIC, I would imagine this should work but I should not have to do this.
Is there some headers and /or terminators sent as standard with COM1.
Is there a chance that the TTL terminals are only 3.3volt tolerant as I am using 5 volt PIC. I may use a series resistor and see what happens.
It would be great to get to the bottom of this.
Samncw