help with the micro camera

Hi, I’m 1) girl 2) from software - I know that is no the excuse but…))

need help in building the micro camera that is connected with the sd card and make pictures by push of the button…

was thinking to buy this as a start point… https://www.sparkfun.com/products/11868

What should I do with it to make it work how I want

Inga

Buy a key fob cam with an SD card.

Done…

lalunalalol:
Hi, I’m 1) girl 2) from software - I know that is no the excuse but…))

need help in building the micro camera that is connected with the sd card and make pictures by push of the button…

was thinking to buy this as a start point… https://www.sparkfun.com/products/11868

What should I do with it to make it work how I want

Inga

That camera does not need to be built. It is ready to go and just plugs into the camera port on the Raspberry-Pi board.

There is also software ready to go to use this camera on the R-Pi.

Now the R-Pi does have an SD card but this is used for the R-Pi’s OS and system files. You can save images to this SD card but this is not recomended.

The R-Pi has a couple of USB ports and it would be better to use a USB Flash drive to save images.

Now if you just want a camera to record to an SD card skimask gave the answer.