HELLO FRIENDS A QUESTION. I HAVE 2 SparkFun RTK Facet TO USE THEM AS RTK SURVEYING EQUIPMENT, THROUGH HOLYBRO RADIOS SiK Telemetry Radio V3 500mW 915MHz WHAT HAPPENS IS THAT WHEN I TURN ON THE FACET EQUIPMENT I PLACE ONE IN BASE AND THE OTHER IN ROVER AND CONNECT THE HOLYBRO RADIOS. THE RTK DOES NOT CONNECT IT IS AS IF THE RADIOS WERE NOT CONNECTED AND THEY DO NOT GIVE ME THE FIXED RTK SOLUTION. THERE ARE TIMES THAT IF IT CONNECTS AND BEING CLOSE THEY STILL DISCONNECT AND I GET DGNSS. THING THAT IF I CONNECT AND DISCONNECT THE RADIOS SOMETIMES THE FIXED SOLUTION IS RECOVERED BUT MANY TIMES IT IS NOT RECOVERED AND IT IS VERY TEDIOUS, I DON’T KNOW IF YOU CAN SUPPORT ME WITH ANY ADVICE JUST THAT IF I NEED HELP TO CONTINUE WORKING WITH THEM
The SiK radios have a lot of configuration items via the AT commands.
These need to be consistent between radios.
Perhaps narrow the usable band/channels so the hopping syncs quicker.
Generally I found them to be somewhat hit and miss in syncing, so sometimes a restart was the quickest way to get there.
Pick Air and Baud rates which are most appropriate to the volume of data being moved.