I have been working with the ZED-F9R module with an Arduino using the GNSS library from Sparkfun and it is working just fine, I wanted to set it up with an STM32 Nucleo-H7A3ZI-Q board. What changes do I have to make to the library to deploy it on the STM board using the cubeIDE?
Quite a few… To port an Arduino library to work with the STM32 Nucleo-H7A3ZI-Q board using CubeIDE, you need to make the following key changes:
- Replace Arduino-specific libraries with their STM32 HAL equivalents:
-
Replace
Wire.hwithstm32h7xx_hal_i2c.hfor I2C -
Replace
SPI.hwithstm32h7xx_hal_spi.hfor SPI -
Replace
Serial.hwithstm32h7xx_hal_uart.hfor UART
- Modify the library code to use STM32 HAL APIs instead of Arduino APIs. For example:
-
digitalWrite()becomesHAL_GPIO_WritePin() -
analogRead()becomesHAL_ADC_GetValue() -
delay()becomesHAL_Delay()
-
Configure the required peripherals (UART, I2C, SPI, etc.) in CubeIDE and initialize them in your code using the corresponding
MX_<Peripheral>_Init()functions generated by CubeIDE -
Ensure the library’s timing and delay functions are compatible with the STM32 HAL by either:
-
Replacing them with
HAL_Delay()or a timer-based delay function. -
Adapting the existing delay functions to use a timer peripheral
-
Adjust any pin mappings or configurations specific to the Arduino board to match the STM32 Nucleo-H7A3ZI-Q board’s pinout and peripheral mappings
-
Build and link the modified library with your CubeIDE project, ensuring any required STM32 HAL libraries are also linked
The process can be time-consuming, as you may need to refactor significant portions of the library code to work with the STM32 HAL APIs and peripherals. Thoroughly testing the ported library is also crucial to ensure proper functionality