how to connect LOCOSYS LS20033 GPS to Logomatic v2

I bought another logger from sparkfun. The first thing I did was powering it up from my 5.5volt source with only the sd card connected. The USB led is on… Maybe the first logger wasn’t faulty. Should the USB led stay on when powering the board from 5.5volt (messured to 5.34volt)?

here’s the setup for my gps->osd. should it work with the logger out of the box?

http://static.rcgroups.com/forums/attac … kstork.jpg

If the picture does not work, here’s the forum post:

http://www.rcgroups.com/forums/showpost … stcount=57

Im sure you either A) got it working or B) have gone on to something else entirely. But I was running into the same problem until I switched UART. Instead of TXO1 and RXI1 I went over to TXO0 and RXI0 and everything is running fine. Also I had to change Baud to 7 or 57600. Granted this is much faster than I want to communicate at but at Im happy just to get it working LOL