hello
so we finally got the lassen iQ Datalogger (the complete kit) i pluged all the things together, bought 4 AA batterys at 2500mAh, and powered on.
it blinked, stat1 and stat0 after a moment went black, but the power LED still was on (permanent).
i positioned it near a window so it should get a lock, but even after 30minutes the PowerLED was on.
i checked on the computer and there was the gpscon.txt file, changed the mode to KML, and added the SD back to the logger.
then we took the device in the car, placed it direct under the window, and drove about 2 hours.
when we switched the power on, the stat0/1 were blinking short and the powerLED was on.
it was always on, the powerLED during the whole time, and the stat0/1 were never blinking again after the startup.
when i pluged the SD in the computer, there was like just two sort of files.
the gpscon.txt file, and some gps0.txt gps1.txt etc which were all 0byte files and with nothing in it.
i guess this was when i powered the device on, or pushed the “reset” button.
okey, what exactly does the always-on-powerLED mean?