Since new, i had the Logging icn shown as just 1 vertical bar increasing, i though it was “normal” since i did not have a sd card in that unit. Now that i inserted and it seems the system detects it, the logging icon remains the same.
It should display a small “text file” icon; what size is the SD card?
You can check if there are files on the SD via https://docs.sparkfun.com/SparkFun_RTK_ … nu_system/ which should let you compare
You can check whether the SD card is detected or not from the System Menu (https://docs.sparkfun.com/SparkFun_RTK_ … nu_system/)
If the card is detected, logging will begin if logging is enabled (https://docs.sparkfun.com/SparkFun_RTK_ … a_logging/) and enough satellites are in view to get the current time. From your video, it looks like you have more than enough SIV.
Make sure your SD card is formatted for FAT16. We do not yet support very large cards (64GB or larger) or exFAT formats.
Hi Sparky,
This is the same receiver that screen is freezing, also the logging icon is bugged, sometimes apears rare characters etc. I want to send for inpection, this is i already paid shipping to mx, taxes around 300 dlls, and shipping from mexico to usa is expensive, not considering when you return the unit back to me if you dont put in the invoice is a replacement they are going to make pay 20% taxes from an item previusly bought.
From the 2 units i bought, both have problems, They still can be usable but it’s no more than 20 days bought and im not happy .
Sorry the units are posing a problem! Please contact the return group as they can help you with specifics. I believe we can ship units back to you correctly marked as ‘Repaired’ to avoid double taxation.
This may be a firmware bug: https://github.com/sparkfun/SparkFun_RT … issues/415