LED-TRICOLOR-5050 in sparkfun.lbr

Does anyone know where the above item can be sourced? I’ve designed (and ordered) a PCB that uses a SMT RGB LED with this footprint and pinout and as far as I can tell such an object is not currently sold by sparkfun or anyone else. The closest is COM-10866 at sparkfun or 754-1486-1-ND at digikey which appear to have a similar footprint but both of these have a different pinout from the one in the sparkfun lbr.

The pinout of LED-TRICOLOR-5050 is (as far as I can tell from how it lays out on the board):

  • 1—6 +

  • 2—5 -

  • 3—4 -

with 1,6,2 being the LED anodes and 5,3,4 being cathodes

COM-10866 and 754-1486-1-ND (and a similar one sold by Adafruit) all are configured like this:

  • 1—6 -

  • 2—5 -

  • 3—4 -

any help here would be appreciated - otherwise I may have some detailed board modding to do!

Matt