LG290P - still garbage data / no PQTM replies even after trying every baud rate

What I’m seeing

  • Connected via USB-C (CH342) and directly to an ESP32-S3 (TX1/RX1 pins).
  • Set port to 8-N-1, tried every standard baud from 9 600 → 921 600, including the spec’d 460 800 bps.
  • No matter the rate:
    • Port B (UART1?) = silent.
    • Port A (UART3?) and ESP32 link = endless repeating pattern
      80 00 78 80 78 80 78 … (0x78/0x80/0xF8/0x00).
    • $PQTMVERNO*58<CR><LF> always times out.

What I already verified

  • TX/RX crossover & common ground OK (swapping silences output).
  • Added explicit CR+LF after every command.
  • Tried $PQTMDEBUGOFF*06 and blindly sent CFGPROT/CFGUART strings—no ACK.
  • 3 V3 rail stable; same antenna works on other receivers.

To add to this I also tired to use the QGNSS through the USB-C (UART1) and the only data im getting is this which seems to be garbage also…could I have a bad board?

Did U try to flash the fw?
But use Qgnss 2.1
https://www.quectel.com/content/uploads/2024/07/QGNSS_V2.1_EN.zip
then complete upgrade on esp…

How to connect to the module is described here Interface w/ LG290P - SparkFun RTK Postcard Hookup Guide in the Connecting to the LG290P section.

If the connection is successful, you can try to restore factory settings:

Restore settings to factory defaults
$ PQTMRESTOREPAR*13

If there are no errors, you will receive the foloowing response:
$PQTMRESTOREPAR,OK*3B

To see satellites in QGNSS the antenna must be outside the window.

Switched to the latest version of QGNSS and flashed it with the latest firmware and it all just works now…super weird. So maybe just bad firmware?

I also now have it working while connected to my esp32s3…but feeding 3.3v from the esp32s3 to the BlueSMiRF did not work - I had to feed 5v from the esp32s3 to the 5v on the board before it would start actually exporting the full sentences over UART 2